Mouser Now Stocking SparkFun Artemis Dev Kit with Full Arduino, Bluetooth, and Mbed Support
October 15, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Artemis Development Kit with Camera from SparkFun.
SparkFun Artemis Development Kit with Camera is the latest board to be released around the SparkFun Artemis Module, and it allows access to more software development features than previous Artemis based boards. Recommended software used to program the Artemis Development Kit are the Arduino IDE, Arm® Mbed™ OS (Studio and CLI), and AmbiqSDK. An updated USB interface (NXP MKL26Z128VFM4 Arm Cortex®-M0+ microcontroller) allows the SparkFun Artemis Development Kit to act as mass storage device (MSD), human interface device (HID), and communication port (COM).
The Artemis Module includes a 48-MHz Arm Cortex-M4F processor with an available 96MHz turbo mode. The Cortex core includes with Bluetooth Low Energy 5.0 connectivity and offers low power consumption down to 6 µA per MHz (less than 5 mW). The SparkFun Artemis Module is fully FCC/IC/CE certified with 1 Mbyte of flash and 384 Kbytes of RAM that gives plenty of room for the user's code. The flexibility of the Artemis module starts with an Arduino core. The user can program and use the Artemis module just like they would an Uno or any other Arduino board. Additional functionality stems from the ability of the Artemis Development Kit to run a real-time operating system (RTOS) such as the Arm Mbed OS or the AmbiqSDK.
Attached to the Qwiic I2C bus is a LIS2DH12TR MEMS accelerometer (for gesture recognition) and a digital MEMS microphone. It also includes an edge camera connector for the Himax CMOS imaging camera to experiment with always-on voice commands and image recognition with TensorFlow and machine learning.
To learn more about the SparkFun Artemis Development Kit with Camera, visit https://www.mouser.com/new/sparkfun/sparkfun-kit-17071-artemis-development-kit/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com